ArcFM Utility Network Definition

​The ArcFM Utility Network (UN) Configuration Guide is a collection of concepts, requirements, and recommendations for applying UN-specific models to electric power facility domains. These models are designed to be extensible and lets you create a better collaboration between Esri, utilities, and vendors to lower implementation costs.

Schneider Electric provides custom UN models or asset packages, to make the ArcFM Solution XI series products easier to implement. Any packages that predate Version 4 of the UN are supported, but must be configured to get the most productivity from the solution.

Need more information on UN Terminology? Visit the Esri support topic Utility Network Vocabulary.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.