Locational vs. Functional Equipment

To support the needs of the Utility Network Community (UNC), there needs to be the support of locational and functional equipment. This support means being able to support a single piece of equipment at a single location with known design attributes (Locational) and the current installed attributes (Functional).

Example: A request can be made to change out a transformer, the change out occurs, but for supply reasons the change out process could not replace like equipment for like. They may have needed to temporarily install an oversized transformer. Users would like to track the locational and functional attributes of all transformers, capacitors, circuit breakers, and regulators. There may also be some environmental tracking requirement for oil-filled equipment because of PCB contamination cases.


Recommended Configuration

  • Functional equipment installed is listed in non-spatial object tables, such as ElectricJunctionObject. If the user wants the details of the functional equipment to be exported by the export subnetwork method and moved to the ADMS, containment associations must be created and junction-junction associations between the non-spatial object and the terminals must also exist.

  • Device must live in the E:Has Functional Equipment and E:Functional Equipment network categories along with the record in the non-spatial object tables.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.