Simple Device Network Categories
The entities in this section are modeled as simple, single-terminal features in the device or junction feature class, or no-terminal objects in the JunctionObject table.
Network Categories
|
Equipment Type |
Network Category |
Applicable tables |
Description |
|---|---|---|---|
|
Riser |
E:Riser |
ElectricDevice ElectricJunctionObject |
Applies to a feature or object in the electric junction table that represents a junction in which a span conductor translates from underground to overhead (or vice versa). |
|
Streetlights |
E:Streetlight |
ElectricDevice ElectricJunctionObject |
Applies to a feature or object in the electric device table that represents streetlights. |
|
Lightning Arrester |
E:Lightning Arrester |
ElectricDevice ElectricJunctionObject |
Applies to a feature or object in the electric device table that represents lightning protection equipment. |
|
Fault Indicators |
E:Fault Indicating |
ElectricDevice ElectricJunctionObject |
Applies to a feature or object in the electric device table that represents devices or sensors that indicate where faults are occurring. |
Structure Equipment: Equipment Topology Needs
When a Utility Network (UN) is created, a common domain network named the structure network is included to be shared across different domain networks. One key purpose of a structure network is to support a type of association called structural attachments. Structural attachments provide an efficient method to create a list of structures that support a section or subnetwork.
Network Categories
|
Equipment Type |
Network Category |
Applicable tables |
Description |
|---|---|---|---|
|
Substation Boundary |
S:Substation |
StructureBoundary |
Applies to a feature in the structure boundary table that represents the boundary of substations. |
|
Poles |
S:Pole |
StructureJunction |
Applies to a feature in the structure junction table that represents poles. |
|
Pads |
S:Pad |
StructureJunction |
Applies to a feature in the structure junction table that represents the concrete pad used to install pad mounted equipment. |
|
Cabinets |
S:Cabinet |
StructureBoundary StructureJunction |
Applies to a feature in the structure junction or structure boundary table that represents a pad or wall mounted storage facility for devices and bus connections to a circuit. |
|
Guys & Anchors |
S:Guy |
StructureJunction |
Applies to a feature in the structure junction table that represents guy wire used in supporting poles. |
|
Guys & Anchors |
S:Anchor |
StructureJunction |
Applies to a feature in the structure junction table that represents equipment used to anchor guy wire. |
|
Pole Assembly |
S:Pole Top Assembly |
StructureJuctionObject |
Applies to a feature in the structure junction object table that represents pole top assemblies used for securing conductor to poles (crossarms). |
|
Conduit Manager |
S:Duct |
StructureEdgeObject |
Applies to an object in the structure edge object table that represents a single duct within a duct bank. |
|
Conduit Manager |
S:Duct Bank End |
StructureJunction |
Applies to a feature in the structure junction table that represents the physical position that a duct enters/exits a vault. |
|
Conduit Manager |
S:Duct End Direction Line |
StructureLine |
Applies to a feature in the structure line table that points in the direction that the duct flag is presenting. |
|
Conduit Manager |
S:Duct End Flag |
StructureBoundary |
Applies to a feature in the structure boundary table that represents a duct within a duct flag. This feature must be able represent different duct cross sections and diameters. |
|
Conduit Manager |
S:Duct Flag Leader Line |
StructureLine |
Applies to a feature in the structure line table that forms a visual link from a point on a duct bank to a duct flag that shows the cross-section diagram for the duct bank at that point. |
|
Conduit Manager |
S:Duct Flag Outline |
StructureBoundary |
Applies to a feature in the structure boundary table which contains S:DuctEndFlags while providing a background for visibility of the flags. The outline is the location where duct flag labeling is stored and can be viewed on the map. |
|
Conduit Manager |
S:Vault |
StructureBoundary |
Applies to a feature or object in the structure boundary table that represents a vault that provides access to duct work. |