Equipment Model Topology — Balanced Equipment

In the balanced model, each device and line feature, such as a conductor, can represent up to three different phase-specific components of similar function. We refer to the feature as a bank. In balanced equipment, it is assumed that the units are identical or that the difference between the unit data is not needed to be defined in the GIS.


Recommended Configuration

  • The bank is represented by the ElectricDevice feature.

  • Set the TerminalConfiguration field value on the device(bank) record to All.

  • If units are desired in a balanced network use the network category of E:Has Disconnected Units.

  • If units are not used, define any unit attributes on the ElectricDevice feature.

Example Bank for Balanced Equipment

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.