Required Fields on Electric Devices

These fields will be mapped when using the ArcFM applications. Although the field names are not required, the data type and a field representing this data is required.

Name 

Required 

Data Type 

Description 

Sample Data 

​Phases Normal 

​Yes 

Short or Long ​Integer

​Domain coded value. Bound to an in-line Network Attribute. Used to control phase propagation in electric subnetworks and to inform electric tracing behavior. 

​1 = C 

​2 = B 

​3 = BC 

​4 = A 

​5 = AC 

​6 = AB 

​7 = ABC 

​0 = None 

​VoltageGroup 

​Yes 

Short or Long ​Integer

​Domain coded value.  

 

​LifeCycleStatus 

​No 

Short or Long ​Integer

​Domain coded value. Bound to a Network Attribute. Differentiates between facilities in different operational states, such as in-service, planned, abandoned, etc. Can be used to inform electric tracing behavior. 

 

​AssetID 

​No 

​Text

​Equipment identifier used by the electric utility. Customers can alias this field to FacilityID to avoid adding a new field 

 

​InstallDate 

​No 

​DateTime

​Date the equipment was installed 

 

​Manufacturer 

​No 

​Text

​Generally helpful information. 

 

​Model 

​No 

​Text

​Generally helpful information.  

 

​SerialNumber 

​No 

​Text

​Generally helpful information. 

 

​DesignID 

​No 

​Text

​The link to the ArcFM Designer Design Identifier 

 

​WMSCode 

​No 

​Text

​This field stores the code generated by the integrated WMS; this code is used during removals, as it is the reference for the application to know what specs were installed initially. 

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.