Equipment Network Categories
Equipment type categories are used to identify electrical equipment with respect to its basic function, such as a transformer, switch or conductor. They are also used to identify meaningful subclasses within some equipment types. Membership in an equipment type category often implies a set of applicable attributes. For example, the transformer category feature in a Utility Network (UN) is expected to have a PrimaryConnectionType attribute.
Required Configuration
All categories that apply to any given AssetGroup AssetType combination, both general and specific, should be assigned to that combination. This means that a combination for a fuse type in the device table, should belong to all of the categories shown for this example:
Example - Category assignment for an AssetGroup/AssetType combination in the Device table that corresponds to "fuse"
-
E:Switch
-
E:Switch - Fuse
-
E:Protective
NOTE: For equipment types in the unbalanced model, both the bank and unit will have the same network categories applied to them, differing only by the E:Has Connected Units (bank only) and the E:Unit (unit only) categories.
|
Network Category Name |
Applicable tables |
Description |
|---|---|---|
|
E:Busbar |
Line EdgeObject |
Applies to features in the Electric Line feature class that model busbars. These features must have fields that carry phase and voltage. |
|
E:Conductor |
Line EdgeObject |
Applies to line features that represent conductors. These features must be in the Electric Line feature class and must have fields that carry phase and voltage. |
|
E:Conductor Info |
EdgeObject |
Applies to non-spatial unit objects that belong to a conductor bank (which may be a Line feature or an EdgeObject row). Each object in this category represents a phase conductor or a neutral conductor. |
|
E:Connector Conductor |
Line |
Used to denote conductors used to connect spatial features instead of using junction to junction connectivity associations. |
|
E:Connection - Tap |
Junction |
Applies to a feature or object in the Electric Junction table that is used modeling transformers with the E:Transformer — Tap Network Category. |
|
E:Distributed Energy Resource |
Device JunctionObject |
Applies to a feature or object in the Electric Device table that represents a distributed energy resource (i.e. solar arrays, generators, batteries). |
|
E:Fault Indicating |
Device |
Applies to a feature or object in the Electric Device table that represents devices or sensors that indicate where faults are occurring. |
|
E:Lightning Arresting |
Device |
Applies to a feature or object in the Electric Device feature class that represents lightning protection equipment. |
|
E:Power Factor Correcting |
Device JunctionObject |
Applies to a feature or object in the Electric Device feature class that compensates for fluctuations in available power and reduces inefficient energy consumption. |
|
E:Power Factor Correcting - Capacitor |
Device JunctionObject |
Sub-category of E:Power Factor Correcting |
|
E:Power Factor Correcting - Reactor |
Device JunctionObject |
Sub-category of E:Power Factor Correcting |
|
E:Riser |
Junction |
Applies to a feature in the electric junction table that represents a junction at the location where a span conductor travels from underground to overhead (or vice versa). |
|
E:Service Point |
Device JunctionObject |
Applies to a feature or object in the electric device or electric junction object table that represents a service point or meter. |
|
E: Critical |
Device JunctionObject |
Applies to a feature or object in the electric device or electric junction object table that represents a critical service point in which supply to power must not be interrupted. |
|
E:Primary |
Device JunctionObject |
Applies to a feature or object in the electric device or electric junction object table that represents a service point that is energized from the primary circuit. |
|
E:Secondary |
Device JunctionObject |
Applies to a feature or object in the electric device or electric junction object table that represents a service point that is energized from secondaries. |
|
E:Streetlight |
Device |
Applies to a feature or object in the Electric Device feature class that represents streetlights. |
|
E:Switch |
Device JunctionObject |
Denotes the main feature or object (as opposed to a unit) that represents a switch bank or device. |
|
E:Switch - Circuit Breaker |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Switch - Disconnect |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Switch - Fuse |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Switch - Load Break |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Switch - Reclosing |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Switch - Sectionalizing |
Device JunctionObject |
Sub-category of E:Switch. |
|
E:Device Controller |
JunctionObject |
Applies to a JunctionObject record that can be contained by another JunctionObject record representing the unit has a device controller. |
|
E:Transformer |
Device JunctionObject |
Applies to a feature or object that represents a transformer bank (this includes a single-phase transformer device, which is modeled as a bank that contains only one unit. |
|
E:Transformer - Step |
Device JunctionObject |
Sub-category of E:Transformer. Applies to a feature or object in the Transformer category whose primary and secondary voltages are in the same general voltage class (typically both MV). |
|
E:Transformer - Open Delta |
Device JunctionObject |
Sub-category of E:Transformer. Applies to a feature or object in the Transformer category whose windings are connected in the open delta pattern. Can be referenced by conditions in trace configurations for any tracing applications that need to give special treatment to open delta transformers. |
|
E:Transformer - Open Wye |
Device JunctionObject |
Sub-category of E:Transformer. Applies to a feature or object in the Transformer category whose windings are connected in the open wye pattern. Can be referenced by Conditions in Trace Configurations for any tracing applications that need to give special treatment to open wye transformers. |
|
E:Transformer - Three Winding |
Device JunctionObject |
Sub-category of E:Transformer. Applies to a feature or object in the transformer category that has 3 windings. |
|
E:Voltage Regulation |
Device JunctionObject |
Applies to a feature or object in the electric device or electric junction object table that represents a voltage regulator. |
|
S:Anchor |
Structure Junction |
Applies to a feature in the structure junction feature class that represents equipment used to anchor the guy wire. |
|
S:Cabinet |
Structure Junction Structure Boundary |
Applies to a feature in the structure junction or structure boundary feature class that represents a pad or wall mounted storage facility for devices and bus connections to a circuit. |
|
S:Guy |
Structure Junction |
Applies to a feature in the structure junction feature class that represents the guy wire used in supporting poles. |
|
S:Pad |
Structure Junction |
Applies to a feature in the structure junction feature class that represents the concrete pad used to install pad mounted equipment. |
|
S:Pole |
Structure Junction |
Applies to a feature in the structure junction feature class that represents poles. |
|
S:Pole Top Assembly |
Structure Junction |
Applies to a feature in the structure junction table that represents Pole Top Assemblies used for securing conductor to poles. |
|
S:Substation |
Structure Boundary |
Applies to a feature in the structure boundary feature class that represents the boundary of substations. |