Conductor Network Categories

​The AssetGroup and AssetType values for conductor features in both the Line feature class and the EdgeObject table in the Electric Domain network should be qualified with respect to the following Network Categories:

Network Category Name

Applicable tables

Description

​E:Conductor

​Line

​EdgeObject

​Denotes a main conductor entity that participates in network topology and represents up to three phases and a neutral, where each one may have one or more physical conductors in parallel. 

​E:Busbar

​Line 

​Denotes a conductor entity that participates in network topology and connects equipment within a substation, a switch cabinet, or any other context where busbar equipment needs to be represented as a conductive path in the electric model. E:Busbar and E:Conductor are mutually exclusive categories. 

​E:Connector Conductor

​Line

​Used to denote conductors that connect spatial features instead of using junction-to-junction connectivity. 

​E:Overhead  

​Line

EdgeObject

​Used to denote conductors installed on overhead poles. 

​E:Underground

​Line

EdgeObject

​Used to denote underground cables.

​E:Submersible 

​Line

EdgeObject 

​Used to denote conductors designed for underwater environments.

​E:Has Conductor Info 

​Line

EdgeObject 

​Used to denote an object that has conductor info records.

​E:Conductor Info  

​EdgeObject 

​Used to represent conductor info records.

Setting Conductor Attributes when NOT using Conductor Info

​The following schema applies to both the Line feature class and the EdgeObject table in the electric domain network, for all types that represent a balanced conductor. This applies to a feature or object type that belongs to the E: Conductor network category only and does not belong to the E:Has Conductor Info network category.

Name

Data Type 

Description 

​Sample Data 

​PhasesNormal

​Short or Long Integer

​A domain coded value bound to an in-line network attribute. Used to control phase propagation in electric subnetworks and feed in to electric tracing behavior.

​1 = C 

​2 = B 

​3 = BC 

​4 = A 

​5 = AC 

​6 = AB 

​7 = ABC 

​0 = None 

​ConductorSize 

​Short or Long Integer

​Domain lookup code for the nominal diameter of the conductive material for the phase conductors.

​1 = “1/0” 

​113 = “1000 kCM” 

​ConductorMaterial 

​Short or Long Integer

​Domain lookup code for the conductive material for the phase conductors. 

​18 = “ACSR” 

​23 = “AA” 

​29 = “Aluweld” 

​NeutralType 

​Short or Long Integer

​Domain lookup code describing the neutral conductor. 

​0 = “None” 

​1 = “Present” 

​3 = “Concentric” 

​NeutralSize 

​Short or Long Integer

​Domain lookup code for the nominal diameter of the conductive material for the neutral conductor. 

​1 = “1/0” 

​113 = “1000 kCM” 

​NeutralMaterial 

​Short or Long Integer

​Domain lookup code for the conductive material for the neutral conductor. 

​18 = “ACSR” 

​23 = “AA” 

​29 = “Aluweld” 

Setting Conductor Attributes with ConductorInfo

​The following schema applies to both the Line feature class and the EdgeObject table in the electric domain network, for all types that represent an unbalanced conductor. This applies to a feature or object type that belongs to both the E:Conductor and the E:Has Conductor Info network category. The PhasesNormal attribute is needed to feed in to the phase propagation in the electric network model. The value must reflect all phases found in the ConductorInfo rows, from the PhasesNormal value that is held by the conductor.

Name 

Data Type 

Description 

Sample Data 

​PhasesNormal 

​Short or Long Integer

​Domain coded value. Bound to an in-line Network Attribute. Used to control phase propagation in electric subnetworks and to inform electric tracing behavior. The PhasesNormal value of an unbalanced conductor should be automatically maintained, from an AutoUpdater as an example, as the union of the PhasesNormal values for all of the ConductorInfo rows that it contains.

​1 = C 

​2 = B 

​3 = BC 

​4 = A 

​5 = AC 

​6 = AB 

​7 = ABC 

​0 = None 

ConductorInfo Attributes

​The following schema applies to the EdgeObject table in the electric domain network. This is where the ConductorInfo units that belong to a topological conductor feature, or object, are stored. Each row has these attributes populated:

Name 

Data Type 

Description 

Sample Data 

​PhasesNormal 

​Short or Long Integer

​Domain coded value. Specifies the electrical phase carried by the physical conductor that this ConductorInfo row represents.

​1 = C 

​2 = B 

​3 = BC 

​4 = A 

​5 = AC 

​6 = AB 

​7 = ABC 

​0 = None 

​ConductorSize 

​Short or Long Integer

​Domain lookup code for the nominal diameter of the conductive material. 

​1 = “1/0” 

​113 = “1000 kCM” 

​ConductorMaterial 

​Short or Long Integer

​Domain lookup code for the conductive material. 

​18 = “ACSR” 

​23 = “AA” 

​29 = “Aluweld” 

​IsNeutral 

​Short or Long Integer

​Domain lookup code to indicate whether this is a neutral conductor. 

​0 = “No” 

​1 = “Yes” 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?