Appendix A: Field Model Name to EUNF Mappings

The following tables demonstrate field model name mappings that can be applied to an out of the box EUNF data model. Field model names that are not present in these tables must be added to that model if the ArcFM UN was not the base. Refer to the attribute sections for each equipment type for more details about the additional fields that must be included to support ArcFM Products.

Common Field Model Name Mappings

Field Model Name

EUNF Field Name (Alias)

Description

PhasesNormal

Phases Normal

Domain coded value. Bound to an in-line network attribute. Used to control phase propagation in electric subnetworks and to inform electric tracing behavior.

VoltageGroup

Nominal Voltage (L-G)

Domain coded value. Represents the line to ground voltage on the device or conductor.

LifeCycleStatus

Lifecycle Status

Domain coded value. Bound to a network attribute. Differentiates between facilities in different operational states, such as in-service, planned, abandoned. Can be used to inform electric tracing behavior.

FacilityID

Asset ID

Equipment identifier used by the electric utility.

InstallDate

Install Date

Date the equipment was installed

Manufacturer

Manufacturer

Text description of the manufacturer for the equipment.

Model

Device Model

Text description of the equipment’s model. Generally helpful information.

Conductor Field Model Name Mappings

Field Model Name

EUNF Field Name (Alias)

Description

ConductorSize

conductor_size

Domain lookup code for the nominal diameter of the conductive material.

ConductorMaterial

conductormaterial

Domain lookup code for the conductive material.

Switchable Device Field Model Name Mappings

Field Model Name

EUNF Field Name (Alias)

Description

DeviceStatus

Normal Operating Status

Open Closed state of the device (N/A for banks).

MaxOperatingVolts

Maximum Operating Voltage

Max Voltage rating in volts.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.