Distributed Energy Resource Network Categories

Equipment Type

Network Category

Applicable tables

Description

Service Location

E:ServicePoint

ElectricDevice

Defines the equipment as a service location.

Primary Service Location

E:Primary

ElectricDevice

Applies to a feature that represents a service point that is energized from the primary circuit.

Secondary Service Location

E:Secondary

ElectricDevice

Applies to a feature that represents a service point that is energized from secondaries.

Meter

E:Meter

ElectricJunctionObject

Defines the equipment as a meter.

Distributed Energy Resource

E:Distributed Energy Resource

ElectricJunctionObject

Electric Device

Defines DER Equipment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?