Voltage Regulator Network Categories

Equipment Type

Network Category

Applicable tables

Description

Voltage Regulators

E:Voltage Regulation

ElectricDevice

Electric Junction Object

Applies to a feature in the Electric Device table that represents a voltage regulator, as well as to all JunctionObject Asset Groups and Asset Types that represent a contained, phase-associated unit (which may be a single-phase unit or a three-phase unit) of a voltage regulator bank

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?