Equipment Topology

The Esri Utility Network (UN) model allows a single spatial feature to have multiple terminals that can be connected to a large network of non-spatial edge and junction entities. The ArcFM UN explicitly rejects any free and open-ended use of these capabilities, and instead uses the bank unit pattern to connect entities between terminals of a device. Device modeling must follow this topology.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.