ArcFM UN Configuration Revision History

Revision history of the ArcFM Configuration for the Utility Network. These topics cover content in version 1.3.

Change

Link

Version

Date

Initial Release

 

1.0

5/8/2023

Updated Network Categories Names that were not consistent between sections

Various Places

1.1

9/1/2023

Setting the Spatial Reference

Spatial Reference

1.1

9/1/2023

Updated Formatting

Various Places

1.1

9/1/2023

Conduit Manager Conductor

Conduit Manager Network Category

1.1

9/1/2023

Voltage Regulator

Voltage Regulator Attributes

1.1

9/1/2023

Connecting Conductor (Junction to Junction Connectivity)

Conductor Paths

1.1

9/1/2023

Change to Conductor Units (E:Has Conductor Info)

Conductor Paths

1.1

 

Changes to Units (E:Has Connected Units, E:Has Disconnected Units)

Units in the Balanced and Unbalanced Model

Switchable Devices

1.1

9/1/2023

Changes to Conductor Section to use (E:Has Conductor Info)

Conductor Paths

1.1

9/1/2023

Fix links to the Esri Documentations

Multiple Places

1.1

9/1/2023

Transformer Units

Transformers

 

9/1/2023

CSP Transformers

The Step Transformers for Distribution section updated to note options with and without ADMS/DXI

1.1

9/1/2023

Structural Attachments

Structural Attachments

1.1

9/1/2023

Updated Language as Needed to correct Spellings, Grammer, and overall refresh to simplify

Throughout

1.2

5/24/2024

Terminal Name Restrictions

Removed from Getting Started Section, no longer required

1.2

5/24/2024

Added Diagrams to Clarify Balanced and Unbalanced Network Examples

Added Diagrams that compare Balanced and Unbalanced Topology

1.2

5/24/2024

Combined Balanced and Unbalanced Sections

Balanced and Unbalance topology

 

5/24/2024

Added Examples in Composite Equipment

Added More Diagram and Examples in the Composite Equipment Section, including MV/LV Balanced Transformer Center

1.2

5/24/2024

Updated the Voltage Group Section

Clarify needs for ADMS and Designer in the Voltage Group section.

1.2

5/24/2024

Added New Section on How to Model Service Points

How to Model Service Locations, Premise, and Meters NOTE: Network Category Change

1.2

5/24/2024

Added New Section on How to Model Distributed Energy Resources (DERs)

Modeling DERs

1.2

5/24/2024

Add New Section on how to Model Device Controllers

Controllers within Devices, Added E:Device Controller

1.2

5/24/2024

Removed Product Limitations with Current Releases

New Releases of ArcFM Designer, Feeder Services and Editor where released this spring, Product Limitations will be available during product implementations.

1.2

5/24/2024

Updated Delta Transformer Section to include Topology Diagram

Delta Transformers

1.2

5/24/2024

Removed 3 Winding Transformer Modeling

The ArcFM UN team is in the process of reviewing how to implement 3 winding transformers.

1.2

5/24/2024

Added GangOperated Attribute for Switchable Devices for Unbalanced Network

Switchable Devices Attributes

1.2

5/24/2024

Replaced Attribute Rule Section with Autoupdaters

Out of the Box Autoupdaters

1.2

5/24/2024

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?