DOCA0218EN-00

Tripping Curves

Long-Time and Instantaneous Protection (MicroLogic 2.0 A/E)

Long-Time, Short-Time and Instantaneous Protection (MicroLogic 5.0 A/E, 6.0 A/E and 7.0 A)

Ground-Fault Protection (MicroLogic 6.0 A/E)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.