DOCA0218EN-00

Presentation

Quick View on MicroLogic E trip units allows the operator to quickly view the most important electrical measurements (currents, voltages, active power, energy) without having to touch the trip unit keypad.

The screens automatically scroll in a circular manner so that the operator can view all the main electrical measurements one after another.

The current bargraph and overload LED remain visible at all times in Quick View mode.

Quick View Screen Descriptions

Quick View can be used to display the screens defined in:

  • The factory configuration

  • A custom configuration

Screens Defined in the Factory Configuration

MicroLogic E trip units come with a factory Quick View configuration including the following 9 screens, displayed in the indicated order:

  1. Current of phase 1/A

  2. Current of phase 2/B

  3. Current of phase 3/C

  4. Voltage: phase-to-neutral (V1N) or phase-to-phase (V12)

  5. Voltage: phase-to-neutral (V2N) or phase-to-phase (V23)

  6. Voltage: phase-to-neutral (V3N) or phase-to-phase (V31)

  7. Total active power

  8. Active energy: whole number part (up to 6 digits) in MWh

  9. Active energy: last digit of whole number part plus 3 digits of decimal part

For more information about defining the screens to be displayed in Quick View, refer to Customizing Quick View.

Each screen is displayed for 2 s before being replaced by the next in the list. This duration can be adjusted from 1 s to 9 s in 1 s steps. For more information, refer to Measurement Settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.