DOCA0218EN-00

Displaying Total Active Energy

The total active energy (Ep) consumed since MicroLogic E energizing is displayed on one or two screens:

  • The first screen displays the whole number part of total energy in MWh

  • The second screen displays the decimal part of total energy in MWh.

Example: display of Ep = 26.233 MWh (26233 kWh)

Display of whole number part of total energy in MWh (up to 6 digits)

Display of decimal part of total energy in MWh (up to 3 digits after the decimal preceded by the last digit of the whole number part)

Press to go to screen for the decimal part.

Press to go to screen for the whole number part.

The total active energy (Ep) is calculated and displayed positively whatever the value of the parameter power sign. The maximum total active energy that can be displayed is 999 999 999 MWh. If the total active energy keeps increasing, the value displayed remains at 999 999 999 MWh.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.