DOCA0218EN-00

Instantaneous Protection

  • The instantaneous-protection function helps to protect the distribution system against solid short-circuits. Contrary to the short-time protection function, the time delay for instantaneous protection is not adjustable.

    The tripping order is sent to the circuit breaker as soon as current exceeds the set value, with a fixed time delay of 20 milliseconds.

  • This function carries out true rms measurements.

Instantaneous Pickup

MicroLogic 2.0 A/E

Pickup

(accuracy ± 10 %)

Isd = Ir x ...

1.5

2

2.5

3

4

5

6

8

10

MicroLogic 5.0 A/E, 6.0 A/E, 7.0 A

Pickup

(accuracy ± 10 %)

Ii = In x ...

2

3

4

6

8

10

12

15

OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.