DOCA0218EN-00

Displaying Protection Settings

Protection settings Availability per MicroLogic trip unit type Action Setting display (examples shown are MicroLogic P screens)

2.0 A

2.0 E

5.0 A

5.0 E

6.0 A

6.0 E

7.0 A

Long-time current setting Ir

Press to select Settings menu.

The Ir value is displayed first.

Long-time time delay tr

Press to display tr value.

Short-time pickup Isd

Press to go on to the short-time Isd value.

Short-time time delay tsd

Press to go on to the tsd value.

Instantaneous pickup Ii

Press to go on to the instantaneous Ii value.

Ground-fault pickup Ig

Press to go on to the Ig value

or...

Earth-leakage pickup IΔn

...the IΔn value.

Ground-fault time delay tg

Press to go on to the tg value

or...

Earth-leakage time delay Δt

...the Δt value.

         

Press to return to the beginning of the menu.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.