DOCA0218EN-00

Customizing Quick View

Custom Quick View Configuration

The Quick View factory configuration includes the nine screens presented in the detailed topic.

It is possible to change some or all of the screens of the factory configuration, up to a maximum of ten screens.

If all Quick View screens are removed, pressing briefly will have no effect. The display remains in Tree Navigation mode.

Removing a Screen

Follow this procedure to remove a screen from Quick View:

  1. Make sure you are in manual control of the Quick View mode, and if necessary, press briefly (< 1 s) to activate automatic scrolling and then press briefly (< 1 s) to activate the manual control of the Quick View mode.

  2. When the screen to be removed appears, press and hold (> 4 s).

  3. When the message OK dEL is displayed, the screen has been removed.

Adding a Screen

Follow this procedure to add a screen (selected from the navigation tree):

  1. Access Tree Navigation mode.

  2. In this mode, display the screen you want to add, as described in Tree Navigation.

  3. When the selected screen is displayed, press and hold (> 4 s).

  4. When the message OK Add is displayed, the screen has been added to the Quick View configuration. It is placed in the last Quick View position.

NOTE: If you try to add a screen to an existing configuration that already has ten screens, the message QV full is displayed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.