DOCA0218EN-00

Measurement Ranges and Accuracy

The accuracy of the current measurements depends on both the value displayed (or transmitted) and the circuit-breaker rating (In):

  • Below 0.1 x In, measurements are not significant

  • Between 0.1 x In and 0.2 x In, accuracy changes linearly from 4 % to 1.5 %

  • Between 0.2 x In and 1.2 x In, accuracy = 1.5 %

The resolution for the current is one Ampere.

The resolution for the voltage is one Volt.

The resolution for power is one kW, kVar, kVA.

The resolution for energy is one kWh, kVarh, kVAh.

Measurement

MicroLogic

Accuracy at 25 °C

Measurement range for specified accuracy

Instantaneous current

I1, I2, I3

A, E

±1.5 %

0.2 x In ... 1.2 x In

IN

A, E

±1.5 %

0.2 x In ... 1.2 x In

I ground

A, E

±10 %

0.2 x In ... In

I earth leakage

A, E

±1.5 %

0 to 30 A

Current maximeters

I1 max, I2 max, I3 max

A, E

±1.5 %

0.2 x In ... 1.2 x In

IN max

A, E

±1.5 %

0.2 x In ... 1.2 x In

Demand current

I1, I2, I3

A, E

±1.5 %

0.2 x In ... 1.2 x In

IN

A, E

±1.5 %

0.2 x In ... 1.2 x In

Demand current maximeters

I1max, I2 max, I3 max

A, E

±1.5 %

0.2 x In ... 1.2 x In

IN max

A, E

±1.5 %

0.2 x In ... 1.2 x In

Phase-to-phase voltages (3 and 4-wire systems)

V12

E

±0.5 %

100 ... 690 V

V23

E

±0.5 %

100 ... 690 V

V31

E

±0.5 %

100 ... 690 V

Phase-to-neutral voltages (4-wire systems)

V1N

E

±0.5 %

100 ... 690 V

V2N

E

±0.5 %

100 ... 690 V

V3N

E

±0.5 %

100 ... 690 V

Average voltage

Vavg

E

±0.5 %

0 ... 100 %

Voltage unbalance

U unbal

E

±0.5 %

0 ... 100 %

Instantaneous power

P (per phase)

E

±2 %

30...2000 kW

Q (per phase)

E

±2 %

30...2000 kVar

S (per phase)

E

±2 %

30...2000 kVA

Power maximeters

P max (per phase)

E

±2 %

30...2000 kW

Q max (per phase)

E

±2 %

30...2000 kVar

S max (per phase)

E

±2 %

30...2000 kVA

Demand power

P (per phase)

E

±2 %

30...2000 kW

S (per phase)

E

±2 %

30...2000 kVA

Demand power maximeters

P max (per phase)

E

±2 %

30...2000 kW

Instantaneous power factor

PF

E

±2 %

0 ... +1

Total energy

Ep

E

±2 %

-1010 GWh ... +1010 GWh

Eq

E

±2 %

-1010 GVArh ... +1010 GVArh

Es

E

±2 %

-1010 GVAh ... +1010 GVAh

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.