DOCA0218EN-00

MicroLogic A Trip Unit Setting Procedure

  • Briefly press to scroll through the possible settings for a given parameter.

  • Press and hold to save the setting and go on to the next parameter.

  • After selecting the language, press and hold to return to the Metering menu.

  1. From the Metering menu, simultaneously press the two buttons to access the parameter settings for the communication option.
  2. Select the desired Modbus address.
  3. Press and hold to save the setting and go on to the next parameter.
  4. Select the desired baud rate.
  5. Press and hold to save the setting and go on to the next parameter.
  6. Select the desired parity setting.
  7. Press and hold to save the setting and go on to the next parameter.
  8. Select the desired language.
  9. Press and hold to return to the Metering menu.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.