DOCA0218EN-00

Earth-Leakage Protection on MicroLogic 7.0 A Trip Unit

  • The earth-leakage protection function primarily protects people against indirect contact because an earth-leakage current can provoke an increase in the potential of the exposed conductive parts.

  • The earth-leakage pickup value IΔn is displayed directly in amperes and the time delay follows a constant-time curve.

  • An external rectangular sensor is required for this function.

  • This function is inoperative if the long-time rating plug is not installed.

  • As a type-AC, the circuit breaker is protected against nuisance tripping.

  • As a type-A, the circuit breaker provides DC-component withstand up to 10 A.

Earth-Leakage Pickup Value IΔn

IΔn pickup (A) (accuracy 0 to -20 %)

0.5

1

2

3

5

7

10

20

30

Time Delay Δt

Δt time delay settings (ms)

(Maximum resettable time)

60

140

230

350

800

Δt maximum break time (ms)

140

200

320

500

1000

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.