DOCA0218EN-00

Resetting Current Maximeters

  1. Select the maximum current value to be reset (for example, I2 max.) by pressing as many times as required to access the I2 max. screen.
  2. Reset by pressing and holding down for 3 to 4 seconds. The old value changes to the present value (the new maximum).
  3. Select another value of current to reset or return to the main menu by pressing as many times as required to select another maximum value to reset or return to the main menu.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?