DOCA0218EN-00

MicroLogic A Settings

Communication Settings

When the BCM ULP communication module is installed, the communication settings must be set.

The communication parameters have default values that can or must be changed according to the needs of the installation or users.

The following table lists the communication parameters and indicates their possible values.

Parameter

Definition

Format (X=digit)

Default value (units)

Default value screen

Possible values

Modbus address Unique Modbus address of MicroLogic A trip unit on the Modbus network to which it is connected. XX 47 1 to 47
Baud rate Number of kbits/s (kbauds) exchanged on the Modbus network. It must be set to the same value for all devices on the network. XX.X 19.2 (kb) 9.6/19.2
Parity Used for error checking based on the number of bits in the transmitted data group. E or n E

E (Even)

n (none)

Language Work language for the screens En or Fr En

En (English)

Fr (French)

For more information about installing and setting the BCM ULP communication module, consult the instruction sheet on the Schneider Electric website: 5100512864A

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.