DOCA0218EN-00

Trip History for MicroLogic E Trip Unit

The trip history of MicroLogic E trip units can be used to analyze circuit breaker tripping, thereby increasing the overall availability of your installation.

The trip history displays the list of the last 10 trips.

For each trip, the following indications are recorded and displayed:

  • The tripping cause: Ir, Isd, Ii, Ig or Auto-protection (Ap) trips

  • The date and time of the trip (requires communication option) in order to set Date and Time

List of trip causes:

  • Overloads (Ir)

  • Short-circuits (Isd or Ii)

  • Ground faults (Ig)

  • Auto-protection (Ap)

For more information, refer to Displaying Trip History.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?