DOCA0218EN-00

Using Quick View

Activating and Deactivating Quick View

  • When energized for the first time, the MicroLogic E trip unit automatically activates Quick View and scrolls through the factory-configured screens.

  • Press briefly (<1 s) to activate the classical tree navigation mode. Press again briefly (<1 s) to return to Quick View mode.

  • In both Tree Navigation and Quick View modes, the first screen displayed is screen 1, but in tree navigation mode, finally the screen changes to display the instantaneous current of the most heavily loaded phase.

Manual Control of Quick View Scrolling

Automatic scrolling of Quick View screens can be paused, for example to display a screen for more than 2 s in order to make a note of measurements.

Press briefly (< 1 s)

Stops scrolling and displays the present screen for 20 s if no other action is taken.

It is then possible to manually scroll through each Quick View screen one after the other.

Press briefly (< 1 s)

Displays the next screen for 20 s if no other action is taken.

Returning to Automatic Scrolling

After a period of 20 s with no action, automatic scrolling is reactivated.

Events Causing the Interruption of Automatic Scrolling

Automatic scrolling of Quick View screens is also interrupted by the following events:

  • Tripping (interrupted until the trip is reset by pressing )

  • Change in a protection setting

  • Battery test (while the test button is pressed).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.