DOCA0218EN-00

HMI Display Modes

Definitions

  • MicroLogic A trip unit has a single display mode: Tree Navigation mode to access data through a menu structure.

  • MicroLogic E trip unit has two display modes:

    • Tree Navigation mode to access all data through a menu structure

    • Quick View mode to display a selection of data

Tree Navigation Mode

In Tree Navigation display mode, use the buttons below the display screen to navigate in the menu structure. Tree Navigation display mode presents a single network of menus, with monitoring values and editable configuration settings.

Refer to Navigating Using the Keypad Buttons for more information about how to use the keypad buttons to:

  • Navigate the menu structure

  • Access and edit settings

For more information about the menu structure and settings , refer to Tree Navigation Mode.

Quick View Mode

MicroLogic E trip unit also offers a Quick View mode. Quick View mode displays up to 10 screens automatically one after the other, with a configurable time delay. An override function is available to allow manual scrolling.

Quick View is the factory-set display mode for MicroLogic E trip unit.

You can modify the Quick View screens defined in the default configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.