DOCA0218EN-00

Long-Time Protection

The long-time protection function protects cables (phases and neutral) against overloads. This function is based on true rms measurements.

Thermal Memory

The thermal memory continuously accounts for the amount of heat in the cables, both before and after tripping, whatever the value of the current (presence of an overload or not). The thermal memory optimizes the long-time protection function of the circuit breaker by taking into account the temperature rise in the cables. The thermal memory assumes a cable cooling time of approximately 15 minutes.

Setting the Ir Pickup

The Ir pickup setting values depend on the long-time rating plug inserted in the MicroLogic A/E trip unit. For more information, refer to Long-Time Rating Plug.

Ir pickup = setting value x In rated current.

As standard, trip units are equipped with the standard rating plug (0.4–1 x In).

Rating plug

Current setting

Standard

0.4

0.5

0.6

0.7

0.8

0.9

0.95

0.98

1

Low-setting option

0.4

0.45

0.50

0.55

0.60

0.65

0.70

0.75

0.8

High-setting option

0.80

0.82

0.85

0.88

0.90

0.92

0.95

0.98

1

Off-plug

No long-time overcurrent protection (Ir = In for Isd setting)
NOTE: The long-time rating plug must always be removed before carrying out insulation or dielectric withstand tests.

When the current is higher than Isd or Ii, only short-time overcurrent protection and instantaneous protection are operational.

Setting the tr Time Delay

The time delay settings indicated on the rating plugs correspond to the tripping times for an overload of 6 x Ir in cold-state conditions.

The table below gives tripping times according to tr time delay.

Tripping time (s)

Accuracy

tr time delay

0.5

1

2

4

8

12

16

20

24

at 1.5 x Ir

0 to -30%

12.5

25

50

100

200

300

400

500

600

at 6 x Ir

0 to -20%

0.5

1

2

4

8

12

16

20

24

at 7.2 x Ir

0 to -20%

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.