DOCA0184EN-01

Graphical View

You can connect different switchboards together under Graphical view (B). Once you connect, they will be displayed under CONNECTED SWITCHBOARD (J).

Graphical view

To connect:

  1. Select Graphical view.

  2. Find the Switchboard cards (L) under Workbench (M), Drag the cards to the area marked with the icon and release to add them.

  3. If you want to move the switchboard back to the Workbench, click > Move to workbench (N).

NOTE: Graphical view will be activated only after you create a switchboard under List view.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.