DOCA0184EN-01

Manage the Projects

Once logged in, you can create or load a project from the home page:

Manage the projects

  • To create a new project, click Create your project (A). For more information, refer to Create a Project.

  • To load a previously saved project, do the following:

    1. Click Load a project (.zip) (B).

    2. Select the project file (.zip) from your system.

    3. Click Open. Now the project opens.


For existing projects, do the following:

  • My Projects (C): Displays projects created by you.

  • Reference design (D): Displays reference projects provided as pre-made. For more information, refer to Reference Design.

  • All Projects (E): Displays projects from both My Projects and Reference design.

To view existing projects, click Open (F).

You can do following (G) for existing projects:

  • To share the project, click > Share via link. Select one of the following options:

    • Copy link: To share the project through a sharable link..

    • Email link: To share the link via email.

  • To duplicate the project, click > Duplicate.

    Update the project name and click Confirm.

  • To export the project to your local device, click > Export as file.

    The file is saved in your device in .zip format at your default download location.

  • To delete the project click > Delete and then click Confirm.

    The selected project is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.