DOCA0184EN-01

Assign a Pictogram

To add pictogram for the devices, do the following:

Label Editor

  1. Click Select Pictogram (E).

  2. In Pictogram Selection box (F), select the required icon, and click Confirm.

    NOTE: You can select multiple devices from Row devices setting and assign the same pictogram to all of them at once.

  3. To print labels for the devices, click Print Preview tab (G).

  4. In Print Setting (H) section do the following:

    • Select the type of print

    • Select the page type

    • Select the page size

  5. To print and save the labels from your computer, click on print or save icons (K) section or you can print from the DOCUMENT tab.

    Print Preview

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.