DOCA0184EN-01

Select the Enclosure

The FRONT VIEW (A) tab displays the compatible enclosure ranges based on the required space to mount the devices configured previously. You can find module information in the DEVICES TO MOUNT (B) section.

Select the enclosure

  1. To refine your search, update the following sections:

    • SPARE SPACE (C): Select the modular reserve as per your requirements.

    • GENERAL CHARACTERISTICS OF THE ENCLOSURE(D): Select the general characteristics of the enclosure based on your requirements.

  2. Select the enclosure from Functional, Universal, and Modular category (E) and click Next (F).

    NOTE: You can only select enclosures which are compatible. Enclosure marked with an orange notification are not compatible with the type of modules to be mounted.
  3. On the next page, select the detailed characteristics of the enclosure and click Next.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.