DOCA0184EN-01

Print Preview

Print preview enables you to visualize the number of printed pages related to the single line diagram. The number of pages can be optimized according to the number of columns and devices displayed per page and the level of readability requested.

Use the zoom in , zoom out , and fit to page options to set up the number of pages.

To generate PDF output, do the following:

  1. Click Export SLD as PDF.

    NOTE: A warning message will appear if there is any empty role card in the diagram. Select Yes to delete the empty role card from SLD.

  2. Enter details in Version and Modification fields, then click Generate.

The generated PDF includes the following:

  • Cover page with company information, project details, and a table of electrical characteristics.

  • Single line diagram.

  • Footer on each page showing the project name, creation date, and page number

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.