DOCA0184EN-01

Standard View

In Standard view (A), you can view the single line diagram with functional markers generated.

Standard view

Functional markers are combination of a letter and number. The letters are generated as following:

Protection Device Switch Other Device
Q mark I mark X mark

Three numbering modes are available to view the diagram with functional markers:

  • Incremental Automatic (B): The functional marker generated consists of a letter and a number. The number indicates the device's position in the diagram from left to right, and for devices in the downstream circuit, it indicates the position from top to bottom.

    NOTE: At the top right of the screen, there is a lock icon (E) that freezes the numbering. This allows changes to the single line diagram without impacting existing functional markers. Any new markers added after locking will be numbered sequentially from the last number created before locking, regardless of their position. When unlocked, all marks are automatically renumbered based on this principle.
  • Subtree Automatic (C): The functional marker generated consists of a letter and a series of numbers. The numbers correspond to its downstream position in relation to the incomer.

  • Personalization (D): This mode allows you to update functional markers in the diagrams as needed. You can modify up to 10 characters in the text box provided for each device in the diagram.

NOTE: Switching the view mode for the single line diagram removes the functional markers created by the previous mode and replaces them based on the new mode.

Legend (F): This section displays the usage of letters in functional markers and the devices they correspond to. In the case of Personalization mode, you can modify it as per your usage.

Notes (G): In this section, you can write notes that appears in the final output.

Set Vertical aligned text (H) as YES to align the text vertically. This enables to print more pages in Print preview section.

NOTE: This feature is not available for Blue Tariff FR.

Click Export SLD as PDF (J) to generate a PDF for the single line diagram.

A Circuit identification (K) table is present below the single line diagram where you can update a set of characteristics related to each branch of the diagram. The first row displays the designation updated in the diagram tab for each device. You can set Cartridge visibility (L) to NO to hide the table.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.