DOCA0184EN-01

Create a Project

To create a new project, click Create your project.

The following tabs will appear in sequence. Update the details in each tab to finish creating a new project.

Create a project

Tab name

Function

Reference topic

PROJECT INFORMATION (A)

To update basic project information.

Project Information

SWITCHBOARDS (B)

To create and manage switchboards.

Switchboards

DIAGRAM (C)

To create diagram.

Create a New Diagram

SINGLE LINE DIAGRAM (D)

To generate and view the single line diagram.

Single Line Diagram

FRONT VIEW (E)

To select and manage enclosure.

Front View

LABEL EDITOR (F)

To generate label.

Label Editor

BILL OF MATERIAL (G)

To generate bill of material for the final products.

Bill of Material

DOCUMENTS (H)

To generate and upload documents related to the project

Documents

During your project creation, you can:

Icon

Function

(J)

To add notes in your project.

(K)

To download your project.

(L)

To save your project online.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.