DOCA0184EN-01

About eDesign

eDesign is a cloud-based application that simplifies electrical panel design for small buildings and residential projects.

The guided workflow makes it easy to select panel components. Based on the selected configuration, the application automatically recommends the most suitable enclosure by evaluating:

  • Required IP rating

  • Encloser type (Modular, Functional, Universal)

  • Modular reserve capacity

Once the electrical diagram is created using selectors, eDesign automatically generates:

  • Single Line Diagram

  • Component Labels

  • Complete Bill of Material

  • Detailed Project Report

  • Certificate Compilation

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.