DOCA0184EN-01

Mount the Devices in the Enclosure

To mount and unmount the devices in the enclosure, do the following:

Mount the devices in the enclosure

  • On the top-left of the webpage, click Mount all. All the devices from the Workbench (C) will be mounted in the enclosure with their corresponding DIN rail or mounting plate according to the device type. Now, reposition some devices or group of devices to the right place according to your needs.

    NOTE:
    • The mounting order of the devices is the same as the order in the workbench view.

    • There will not be any row break between the group feeder and its downstream devices.

    • If you choose Prisma Set G as the enclosure range, the Mount all function will automatically select the 600 mm width within this range.

  • On the top-left of the webpage, click Unmount all. All the devices from enclosure will move to the Workbench.

Alternatively, to mount the devices, select one or multiple devices (press ) from the Workbench and drag and drop them into the enclosure.

To unmount the devices from the enclosure, select one or multiple devices from the enclosure and drag and drop them to the Workbench.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.