DOCA0184EN-01

Create a New Switchboard

To create a switchboard, do the following:

Create a new switchboard

  1. Click Create a switchboard under List view.
  2. Update the following fields under the ELECTRICAL CHARACTERISTICS (A) section:

    • Switchboard name: * Enter a name for the switchboard.

    • Type of switchboard: * Select the type of the switchboard from the drop-down, either Main Panel or Sub Panel.

    • Phase: * Select the phase as Single phase or Three phases.

      NOTE: When you select the type of switchboard as main panel, three phases will be selected as default phase.

    • Rated current - In [A]: Enter the rated current value.

    • Short circuit current - Isc [kA]: Enter the short circuit current value.

      NOTE: According to NFC 14 – 100 standard calculation, the maximum short circuit value is 20 kA.

    NOTE: Fields marked with (*) are mandatory to fill.
  3. Click Create (B) to create a new switchboard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.