DOCA0184EN-01

Project Information

Update the basic project information under the PROJECT INFORMATION (A) tab. The PROJECT INFORMATION (A) tab has the following sections:


Project information

Section

Description

ELECTRICAL CONTEXT (B)

NOTE: Applicable only for France region.

Update the ELECTRICAL CONTEXT section with the following details:

  • Connection type: * Select Limited power less than 36 kVA (old Blue pricing) or Monitored power less than 250 kVA (old Yellow pricing).

  • Number of phases: * Select Single phase or Three phases.

    NOTE: Three phases is selected by default when you select Monitored power.

CASCADING ASSISTANT (C)

NOTE: Applicable only for France region.

CASCADING ASSISTANT section will be added if you select Monitored power more than 36 kVA.

  • Cascading assistant activated: * Select No or Yes. If you select Yes, Cascading assistant window will open.

PROJECT INFORMATION (D)

Update the PROJECT INFORMATION section with the following details:

  • Project name: * Enter the project name.

  • Address: Enter the address details.

  • City: Enter the city name.

  • Country: Enter the country name.

  • Additional information: Enter additional information if any.

CONTACTS (E)

Update the CONTACTS section with the following details:

  • First name: Enter the first name.

  • Last name: Enter the last name.

  • Role: Enter your role.

  • Email: Enter the email address.

  • Phone: Enter the phone number.

NOTE:
  • You can add more than one contact detail. To add a new contact, click Add a new contact.

  • In case, you want to delete any contact details, Click Delete (F).

NOTE: Fields marked with (*) are mandatory to fill.

Once all the fields are updated, click Create (G) to move to the SWITCHBOARDS tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.