DOCA0184EN-01

Homepage

To open eDesign homepage, do the following:

Homepage

  1. Go to https://edesign-630.se.com/home.

  2. Choose your country from the country list.

  3. Read the ‘Important information’ and ‘Terms and conditions’, and select the check-box. Click Accept to proceed.

eDesign homepage appears. It has following sections:

  • Login (A), for more information, refer to
  • Reference design (B), for more information, refer to Reference Design
  • Top-right menu bar (C), for more information, refer to Top-Right Menu
  • Top-left menu bar (D), for more information, refer to Top-Left Menu
  • Video tips (E), for more information, refer to Video Tips
  • Newsfeed (F), for more information, refer to Newsfeed

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.