DOCA0184EN-01

Toolbars Available in Front View

The FRONT VIEW tab has following toolbars:

Horizontal toolbar

Symbol

Function

To zoom out the product on the screen.

To zoom in the product on the screen.

To fit the product on the screen.

To get a focused view of the part selected in the Build mode.

To rearrange the devices inside the panel according to your needs. You can use this mode after using the Mount all function.

To move the enclosure across the screen.

To view the enclosure in a three-dimensional space. This mode is helpful for viewing upstream and downstream device connections.

To refresh the screen

To download the screen as an image.

To open a fullscreen window.

To open the legend window.

To print the stickers for the devices mounted in the enclosure, each with its label.

Vertical floating toolbar

Symbol

Function

To view the enclosure with only busbars installed.

To view the enclosure with devices installed.

To view the enclosure with the front plates installed.

To view the enclosure with the doors installed.

To view the enclosure with the labels displayed for the devices.

To move the floating toolbar across the screen.

Toolbars available in front view

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.