DOCA0184EN-01

Reference Design

Reference designs are real projects already designed with eDesign small buildings. These projects can be used as templates for the software tool handover. Once registered, the you can copy the projects and modify them.

To open reference design, do the following:

  1. Click Reference Design (A).

    You will find list of reference designs.

  2. To access any of the reference design, click Open (B).

NOTE: You can view reference designs without signing in; however, functionality is limited. For example, you cannot download design outputs such as the project report or single-line diagram.

Reference design

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.