DOCA0184EN-01

Create a New Diagram

To create a new diagram, do the following:

DIAGRAM

  1. Click Design the Panel on the selected switchboard.
    The DIAGRAM tab opens with a basic default diagram.
  2. To modify the diagram, add or remove the product role cards in the diagram. Role cards are available in the Roles section on the left side of the webpage. For more information, refer to Product Role Card.
    1. To add the product role cards in the diagram, drag them to the Add icon (C) and release to add the diagram. Alternatively, you can use the Favorites and Group Favorites functions to effectively add the product role cards in the diagram. For more information, refer to Create a Favorite Products or Create a Group of Favorites.
    2. To duplicate the product role cards in the diagram, click > Duplicate, select number of copies and click Validate.
    3. To remove the product role cards from the diagram, do one of the following options:
      • To add a role card to the Workbench section, click > Move to workbench > Confirm.

      • To delete a role card, click > Delete > Confirm.

    NOTE:
    • The INCOMER (E) role card is included in the default diagram and can not be removed. It can only be substituted with the TRANSFER SWITCH (F).

    • The INCOMER, TRANSFER SWITCH, and GENERATOR PROTECTION role cards can not be duplicated.

  3. Configure the role cards with products. To configure, click the SE Product on the role card. For more information, refer to Configure the Product in the Role Card.
    IMPORTANT:
    • The Downstream multiple circuits role card cannot be configured to add any product, as it is used downstream an outgoer role card to display the corresponding line in the single line diagram.

    • You can also add custom product to your configuration for specific role cards. For more information, see Add Custom Products.

  4. You can do following editing action:
    • Click to undo any operation.

    • Click to redo any operation.

    You can undo and redo up to 10 steps.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.