DOCA0184EN-01

Modify the Enclosure Features

To modify the enclosure features of the selected range, right-click within the enclosure. You will get following options (A) to modify the features:

  • Modify the enclosure

  • Delete the enclosure

  • Manage accessories for enclosure

  • Add an enclosure

  • Modify the enclosure height

To change the enclosure range, do the following:

  1. Click Modify range (B) on the right side of the screen.

  2. Select the new range from proposed enclosure list, select required characteristics and click Next.

    NOTE: If you select a new enclosure range, you need to mount the devices from the Workbench again.

Modify the enclosure features

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.