DOCA0184EN-01

Navigate the Electrical Diagram

You can navigate in the diagram with the following options:

  • Use the Move icon to move the screen in all directions.

  • Use the mini map at the bottom-right to figure out which part of the electrical diagram is displayed.

  • Handle and move the blue rectangle in the mini map to navigate through the electrical diagram.

  • Use Zoom in , Zoom out and Zoom 100% icons to view the diagram effectively. Alternatively, scroll the mouse or touch-pad of the computer to zoom in and zoom out.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.