DOCA0184EN-01

Documents

From the DOCUMENTS tab, you can generate or add different types of project documents.

Documents

To generate the following, refer to the AVAILABLE DOCUMENTS (A) section:

  • Single line diagram

  • Bill of materials

  • Project report

  • CE and PEP certificates compilation of the different devices of the panel under a zip format. An intermediary view allows to get the availability of the different certificates according to the products before downloading the compilation.

  • Generate labels

You can upload documents under the PROJECT DOCUMENTS (B) section. Click Add files (C) and upload documents from your computer.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.