0000649741_01_en

Breaker Status Page

To view the breaker status page navigate to Status > Switchgear

NOTE: Some breakers are optional and might not be available in the system configuration. For the actual breakers used, position and reference designator of the breakers please see the Drawings for that specific system.
Breaker Name in manuals / (in NMC interface) Open Status Closed Status
Rectifier mains breaker /
(Q001 - Charger AC input breaker)
The rectifier mains breaker has been manually opened or has tripped. The rectifier mains breaker is closed.
Battery breaker /
(Q004 - Battery breaker)
One or both battery breakers have been manually opened or have tripped. Always monitors the internal battery breaker, as an option it can also monitor an external battery if the signal is wired in series. All battery breakers are closed.
Output breaker /
(Q003 - Charger DC output breaker)
The output breaker has been manually opened or has tripped. The output breaker is closed.
Module input switches /
(Q_PowerMod - Input power module breakers)
One or more module input switches have been manually opened or have tripped. All module input switches are closed.
Output feeders /
(Q_Dist - Distribution system breakers)
One or more output feeders have been manually opened or have tripped. All output feeders are closed.
Surge arrester /
(Z0XX - Surge arrester breaker)
One or more surge arresters have tripped. All surge arresters are closed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?