0000649741_01_en

Overview of the Command Line Interface

The CLI main menu provides some general information of the system and NMC:

  • Firmware versions

  • Name, contact and location of the system

  • Date and time of the login

  • Current status and up time of the NMC

  • Model of the system

  • Descriptions of a few commands

This is an example of a main menu that is shown when logging in to the CLI:

Schneider Electric                      Network Management Card AOS    vX.X.X.X
(c) Copyright 2022 All Rights Reserved  Gutor Modular UPS DC&AC APP    vX.X.X.X
-------------------------------------------------------------------------------
Name      : System name                               Date : 06/21/2022
Contact   : Contact name                              Time : 11:00:45
Location  : Location name                             User : Super User
Up Time   : 0 Days 0 Hours 7 Minutes                  Stat : P+ N4+ N6+ A+
-------------------------------------------------------------------------------
IPv4               : Enabled            IPv6               : Enabled
Ping Response      : Enabled
-------------------------------------------------------------------------------
HTTP               : Disabled           HTTPS              : Enabled
FTP                : Disabled           Telnet             : Disabled
SSH/SCP            : Enabled            SNMPv1             : Disabled
SNMPv3             : Enabled
-------------------------------------------------------------------------------
Super User         : Enabled            RADIUS             : Disabled
Administrator      : Disabled           Device User        : Disabled
Read-Only User     : Disabled           Network-Only User  : Disabled


Type ? for command listing
Use tcpip command for IP address(-i), subnet(-s), and gateway(-g)

The Stat: field provides a quick overview of the status of the NMC. The table describes each status code.

Status Code: Status Description:
P+ The AOS is functioning properly.
N+ The network is functioning properly.
N? A BOOTP request cycle is in progress.
N- The NMC failed to connect to the network.
N! Another device is using the NMC’s IP address.
A+ The APP is functioning properly.
A? The APP is initializing.
A- The APP is initializing.
A! The APP is not compatible with the AOS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?