How to Log in to the Web Interface
The web interface supports the latest versions of the browsers:
-
Chrome®
-
Edge®
-
Firefox®
Log in to the Web Interface
-
Check that HTTPS or HTTP access is enabled and configured correctly on the NMC card.
NOTE: Only HTTPS is enabled by default. -
Open a supported web browser on a computer.
NOTE: The computer needs to be connected to the same local network as the NMC or the internet if the NMC is connected to the internet. -
In the browser field type the URL to the IP address of the NMC (and web server port if changed) or the DNS name of the NMC.
Example NMC Identifier URL Example With an NMC DNS name that is nmcdnsname https://nmcdnsnameWith an NMC IP address of 139.225.6.133 https://139.225.6.133With an NMC IP address of 139.225.6.133 and specified port of :5000 https://139.225.6.133:5000With an NMC IPv6 address of 2001:db8:1::2c0:b7ff:fe00:1100 and specified port of :5000 https://[2001:db8:1::2c0:b7ff:fe00:1100]:5000NOTE: Changehttpstohttpin the URL if HTTP is used instead of HTTPS. -
Enter the user name and password to log in to the web interface.
-
To log out of the web interface, click Log Off in the top right corner of the window.