0000649741_01_en

File Transfer

File transfer is used both to update the firmware and to download logs. There are two different protocols that can be used with different security options:

  • File transfer protocol (FTP): With FTP the information is transferred as plain text. Use SCP for increased security.

  • Secure copy protocol (SCP): With SCP the information is encrypted. SCP is automatically used when the SSH protocol is enabled and configured and the FTP protocol is disabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?