0000649741_01_en

NMC Firmware

The firmware for the NMC card in a Gutor system consists of one file. Examples of the file name are apc_hw21_gmod_2-1-0-3.nmc3 or apc_hw21_sxw_1-4-0-15.nmc3.

Update the NMC Firmware with SCP

To update the firmware using SCP the NMC needs to have SCP enabled and configured network settings. The NMC and the computer also needs to be on the same network.

  1. From a computer on the same network as the NMC open a command prompt window.

  2. Go to the directory that contains the firmware files and list the files:
    scp apc_hw21_YYY_v-v-v-v.nmc3 apc@xxx.xxx.xxx.xxx:apc_hw21_YYY_v-v-v-v.nmc3 and press Enter to run.

  3. Where YYY is the system type code, v-v-v-v is the version of the firmware file and xxx.xxx.xxx.xxx is the IP address of the NMC.
  4. Wait 20 seconds while the card is rebooting.

Verify Firmware Update

To verify that the firmware update succeeded and to check the firmware version it is possible to:

  • From the NMC web interface navigate to About > Network.

  • Use a SNMP GET to the MIB II sysDescr OID.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?